Vishay Intertechnology 200 V N-Channel MOSFET in PowerPAK® 1212‑8S Offers Industry-Low RDS(ON) to Increase Power Density, Save Energy
TrenchFET® Device Offers Typical RDS(ON) of 61 mΩ and FOM of 854 mΩ*nC in 10.89 mm² Package

Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://wwwtest.vishay.com/
en/company/contacts/
MALVERN, Pa. — Sep. 23, 2020 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new 200 V n-channel MOSFET that offers industry-low typical on-resistance of 61 mΩ at 10 V in the 3.3 mm by 3.3 mm thermally enhanced PowerPAK® 1212-8S package, in addition to improved on-resistance times gate charge — a critical figure of merit (FOM) for MOSFETs used in switching applications — of 854 mΩ*nC. Purpose-built to increase power density, the space-saving Vishay Siliconix SiSS94DN is 65 % smaller than devices with similar on-resistance in 6 mm by 5 mm packages.
The typical on-resistance of the TrenchFET® Gen IV power MOSFET released today is 20 % lower than the next best product on the market in a similar package size, and its FOM is 17 % lower than the previous-generation solution. These values result in reduced conduction and switching losses to save energy. With its compact size, the flexible device allows designers to save PCB space by replacing a much larger MOSFET with the same conduction losses, or a similar sized MOSFET with higher conduction losses.
The SiSS94DN is ideal for primary-side switching for isolated DC/DC topologies and synchronous rectification in telecom equipment, computer peripherals, and consumer electronics; LED backlighting for notebooks, LED TVs, vehicles, and vessels; and motor drive control, load switching, and power conversion for GPS, factory automation, and industrial applications.
The device is 100 % RG- and UIS-tested, RoHS-compliant, and halogen-free.
Samples and production quantities of the SiSS94DN are available now, with lead times of 12 weeks.
###
The DNA of tech™ is a trademark of Vishay Intertechnology.
Media Contact - Bob Decker, Red Pines Group
Phone: 1.415.409.0233
Fax: 1.650.618.1512
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://wwwtest.vishay.com/
en/company/contacts/