Vishay Intertechnology vPolyTan™ Polymer Tantalum Chip Capacitors Bring Reliable Performance to Harsh Operating Conditions
Devices Offer High Temperature to +125 °C, Withstand THB Testing of 85 °C / 85 % RH for 500 Hours

Products mentioned:
T50Media Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
This release in:
- English
- Deutsch
MALVERN, Pa. — Nov. 15, 2021 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of vPolyTan™ surface-mount polymer tantalum molded chip capacitors designed to deliver reliable performance in high temperature, high humidity operating conditions.
Vishay Polytech T50 series capacitors feature a robust design with improved hermeticity for increased protection in harsh environments. The devices offer high temperature operation to +125 °C and withstand temperature humidity bias (THB) testing of 85 °C, 85 % relative humidity for 500 hours. These specifications make the capacitors ideal for decoupling, smoothing, and filtering in the harsh environments of industrial, military, aerospace, and edge computing applications.
Offered in the D case (EIA 7343-30) size, the T50 series features ultra low ESR down to 25 mΩ and ripple current to 3.0 A. The devices offer a wide capacitance range from 10 µF to 330 µF over voltage ratings from 2.5 V to 35 V, and a capacitance tolerance of ± 20 %. The capacitors are RoHS-compliant, halogen-free, and Vishay Green.
Samples and production quantities of the T50 series are available now, with lead times of 12 to 14 weeks. Pricing for U.S. delivery starts at $0.45 per piece.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.® Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
https://twitter.com/vishayindust
https://www.facebook.com/VishayIntertechnology
###
The DNA of techÔ and vPolyTanÔ are trademarks of Vishay Intertechnology.
Media Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
This release in:
- English
- Deutsch